Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

A global IT services and consulting company founded in 2000 as a subsidiary of Deutsche Telekom, T-Systems is one of the largest European IT service companies with global delivery capabilities.

Following its strategic vision to provide cloud services, T-Systems’ need for data center expansion became paramount. To fulfil the company's expectations and meet their clients’ business cases, a combination of requirements needed to be achieved for availability, reliability, security, scalability, transparency, efficiency and sustainability - plus a rapid deployment. Expanding or building a traditional data center in a short timeframe can be a great challenge which requires significant resources. After a thorough analysis, a modular, containerized construction proved to be the ideal option to successfully achieve rapid availability and high scalability; easily allowing for future phases of expansion as well as a staged investment.

"The modular design gives us increased flexibility and scalability for future investment, while immediately offering an array of benefits for our customers," said Núria Berché, Program Manager at T-Systems Iberia. "Vertiv worked with us to deliver true expertise and industry knowledge, positioning us to provide a strong cloud platform that serves both domestic and regional customers in Europe."

Case Summary

Location: Barcelona, Spain

Vertiv Solutions: 

Specially designed and built in the Vertiv dedicated Integrated Modular Solutions facility in Croatia, and later transferred to its location in Barcelona, Spain, the T-Systems data center consists of 38 integrated modules hosting nearly 300 Vertiv Knürr® racks, more than 60 Liebert® thermal management units and a number of AC power systems. The modular infrastructure includes insulation, fire protection, monitoring, and secure access control.

Critical Needs:

Expanding or building a traditional data center in a short timeframe can be a great challenge which requires significant resources. After a thorough analysis, a modular, containerized construction proved to be the ideal option to successfully achieve rapid availability and high scalability; easily allowing for future phases of expansion as well as a staged investment.

Download the Case Study

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner

Language & Location