Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Addressing Challenges to Powering IT at the Network Edge

1. Predicting and managing infrastructure costs

IT demands continue to escalate, but controlling costs becomes more difficult. Investing in an efficient and flexible power solution to manage capital and operating costs is a must.

2. Delivering the availability needed for critical applications

You recognize that your data operations, first and foremost, must be available. Recent studies reveal availability is still the #2 concern for facilities under 5,000 square feet, and the #1 concern for critical spaces up to 10,000 square feet in size. As business demands escalate, your IT systems are enablers to growth. The challenge is to maintain or increase the IT resilience and availability required for the organization to succeed.

3. Improving power system visibility and intelligence

Lack of visibility into the power system’s performance can lead to costly mistakes and business productivity loss. Asking staff to manage power protection in addition to day-to-day responsibilities could hinder productivity and lead to unintended problems.

4. Achieving flexibility and rapid deployment

Chances are your company needs applications and systems to be up and running quickly so it can meet business demands. How do you best add, update, or modify power systems to support changing IT needs across the computing landscape?

 

Learn More



PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner

Language & Location