Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Chorus Taps Vertiv to Boost Wholesaler’s EdgeCentre Colocation Data Centre Capacity

19/3/24

New Zealand’s largest telco wholesaler expands Mount Eden colocation capacity with Vertiv thermal management and power solutions

Auckland, New Zealand [March 19, 2024] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, has helped Chorus expand its colocation offering in New Zealand’s largest city, Auckland, and unlock customers’ computing potential in regional locations using its existing distributed network of telecommunications (telco) buildings.

Chorus is a New Zealand wholesaler of telco infrastructure, operating and owning the largest copper and fibre networks in New Zealand. Since its inception in 2011, the organisation has provided New Zealand’s 90-plus retail service providers (RSP) with services on its copper and fibre networks.

Chorus has undergone a colocation data centre evolution to expand its digital reach, repurposing four existing metro-based telephone exchange facilities into EdgeCentre modular data centre sites. Within these sites, Vertiv™ SmartAisle™ data centre infrastructure has been operating to support the Chorus fibre network. Recently, the wholesaler sought to deepen its Auckland data centre capability – where demand is highest – and added capacity to its Mount Eden EdgeCentre site.

“New Zealand RSPs are increasingly determined to offer wraparounds of cloud managed services, and we want to keep being the wholesaler for their network and hosting service requirements in that relationship,” said Mohammad Hadi, colocation product manager at Chorus. “Mount Eden was our pilot build in 2015, and every rack in that facility has since sold out. To give our customers room to play in today’s digital ecosystem, we needed to expand our capacity in Auckland where customers needed it. This demand led to the significant expansion of the Mount Eden site.”

Chorus re-engaged Vertiv for a modular and scalable data centre solution that would complement the facility’s existing structure. Vertiv carried out the design and implementation of a 23-rack hot aisle containment system with a scalable power range of 50kW to 250 kW. The solution uses refrigerant-based air-cooling modules, robust uninterruptible power supply (UPS) systems, and leverages a state-of-the-art environmental monitoring unit, which tracks energy consumption, alerts teams to potential failures, and rapidly diagnoses problems.

“Our 23 racks of new capacity live in a single row on a back wall – an efficient use of space,” continued Hadi. “That’s relevant because sites such as Mount Eden used to be occupied by large, legacy copper telco equipment. They’re now being replaced with smaller, more sustainable fibre alternatives, and Vertiv is helping us free up new space to put it to other uses.

“We’re now looking at more data centre growth in the region. With close to 600 telephone exchange buildings already dispersed throughout the country, we have a head start in giving regional areas access to the computing power and functionality they currently lack, right at the network’s edge.

“This move will also benefit our customers who are making decisions around resilience. In the unfortunate event of a natural disaster, geographical diversity – where workloads spread across multiple locations – is critical for business resilience,” said Hadi.

“With a combined fibre network and distributed data centres offering, Chorus is making a splash on the digitisation of New Zealand,” said Mark Langford, Head of New Zealand at Vertiv. “We’re proud to offer Chorus confidence throughout its colocation journey. With robust edge solutions, the company is inviting innovation within its existing real estate and trusts our leading design in facilitating scalability alongside the colocation demand curve.”

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

CONTACT

Chloe Curby (for Vertiv)
T +61 429 449 993
E Chloe.curby@watterson.com.au

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner

Language & Location