Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Colovore Deploys Liquid Cooling Solution to Offer Customers Rack Capacities up to 50 Kilowatts

22-10-24

Background

Located in the heart of Silicon Valley, Colovore was created specifically to meet the area’s need for data center infrastructure able to support the next-generation, high-performance computing that has evolved from data-intensive technologies. And by standardizing on Vertiv solutions, the company continues to optimize its server footprint for maximum power, cooling and operating efficiency.

Results

  • Enabled fully-packed, top-to-bottom rack deployments with no wasted or unusable rack unit slots
  • Increased operating and capital efficiency due to significant reductions in required cabinets and data center floor space
  • Achieved lower operating costs with savings passed on to customers
  • Improved cooling effectiveness enabling continued support of advanced applications and higher rack densities densities

Case Summary
Location: Santa Clara, California
Critical Need: The age of connectedness and massive data consumption has boosted the adoption of advanced hardware which requires more power consumption than other data center equipment. For example, graphics processing unit (GPU) servers today routinely draw 1 kW per server rack unit. This increase in power usage coupled with the high operating temperatures of high-density environments required Colovore to implement a robust thermal management solution that would enable compact server footprints that maximize power, cooling and operating efficiency.
Vertiv Solution: IT racks using Vertiv™ Liebert® DCD rack door cooling module


DOWNLOAD THE CASE STUDY

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location