Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Oxigen integrates Vertiv’s free cooling and energy-saving technology into its new high-performance data center

25-2-25

Background

Recently honored with a DCM (Data Center Market) Award in the Sustainability category, Oxigen has made sustainability a core value. In collaboration with Vertiv, it has implemented innovative free cooling technology, setting a new industry benchmark for responsible data center operations.

Results

  • Vertiv’s scalable solutions, provided via partners and directly by Vertiv, enabled Oxigen to efficiently meet its current capacity requirements while planning for future growth.
  • With additional orders placed for the PDU orders and PowerBar IMPb solutions, the expansions are structured into three phases: the first one is complete, the second is ongoing, and the third is projected to conclude by March 2025.
  • Oxigen and Vertiv will extend their collaboration, with plans to install up to 5 additional high-performance Vertiv™ Liebert® AFC chillers to support the data center’s anticipated growth.
Case Summary
​Location:​

Spain

Critical Need:

Oxigen faced a critical challenge of finding a cooling solution that could keep pace with its rapid growth. It needed a system that was not only scalable and reliable but also highly energy efficient. With power demands set to surge as AI and new technologies accelerate, Oxigen sought a partner who could meet its high standards.

Vertiv Solution:
  • Vertiv™ Liebert® AFC chiller
  • Vertiv™ Powerbar iMPB systems
  • Vertiv™ Geist™ rPDUs
  • Vertiv™ Liebert® CRV row-based cooling units
  • Vertiv™ Critical Insight

DOWNLOAD THE CASE STUDY

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location