Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Case Study: EPFL – École Polytechnique Fédérale de Lausanne

12/2/19

The École polytechnique fédérale de Lausanne (EPFL) is – in addition to the many traditional universities and universities of applied sciences controlled by the cantons – one of the two Federal Institutes of Technology in Switzerland and is headquartered in Lausanne.

Since its foundation in 1969, it has become one of the best-known institutions for science and technology in Europe.

Like its sister institute in Zurich, the “ETHZ”, it has three main goals: education, research and technology transfer. Over 14,000 lecturers, researchers and students work, teach and conduct research on the main campus.

Background

To ensure the many different innovative and future-oriented projects being carried out by researchers and students are supported with the appropriate IT equipment, the EPFL has an IT and Building Infrastructure teams made up of around 200 employees. Aristide Boisseau, Head of the Datacenter Operations team, plays a particularly important role. Together with his team, he acts as the interface between the two domains, ensuring a regular exchange of information and smooth processes.

High-performance computers are predominantly used at the EPFL to provide the capacity required for scientific calculations. While the EPFL’s budget for new high performance computers has remained the same over recent years, providers have nevertheless increased the capacity of their products in the data center. As a result, the power density per square meter has risen and the existing ventilation cooling systems have not been able to keep pace with this growth. A new, intelligent solution  capable of adequately cooling the 8-point grid systems was therefore required.

Case Summary
Location:

Switzerland

Vertiv Solutions:
  • Consulting on equipment for a new IT center
  • Liebert Smart Rack PDU MPX
  • Knürr DCD35 air-water cooling doors
Results:
  • Improvement of the power usage effectiveness (PUE) value from 2 to 1.06
  • Space saving of 30% to 50%
  • Reduction of CAPEX and OPEX
Download the Case Study

Related Articles

Amadeus Image

Case Studies

Amadeus
PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location