Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Greenergy and A-Kaabel deploy Vertiv™ rack PDUs to power scalable data center growth in Estonia

31/7/25

Background

Greenergy builds energy-efficient data centers using Estonia’s low carbon energy sources and cold climate to power and cool its facilities. Over time, its vision is to expand operations across the Baltics, harnessing alternative energy sources and proving that high-performance data centers can operate responsibly.

Results

  • Enabled precise measurement of IT load at the customer level and assisted with the capacity optimisation, and meeting EN 50600 standards for climate-conscious operations.
  • Assisted Greenergy to meet target PUE levels with Vertiv’s rPDU solution, supporting long-term energy efficiency.
  • Assisted Greenergy to exceed EN 50600 uptime requirements (99.982%) by operating virtually without interruption for several years.
Case Summary
​Location:​

Estonia

Critical Need:
  • Infrastructure scalability: Meeting accelerated deployment timelines (3-4 months) for large-scale colocation projects (10-20MW capacity) driven by AI workload demand
  • Energy efficiency maintenance: Aiming to reach and sustain a PUE of 1.2 or lower, in line with continuously increasing IT load and rack density.
Vertiv Solution: Vertiv™ rack PDUs

DOWNLOAD THE CASE STUDY

Related Articles

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location