Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv™ Rolls-out Fully-Integrated System for Micro Data Centres Across Europe, Middle East and Africa

21/3/17

Newest SmartCabinet™ offers a turn-key, cost effective and space saving solution that eliminates the need to build complex computer rooms

Southampton, UK [March 21, 2017] – Vertiv™, formerly Emerson Network Power, today announced the rollout of Vertiv SmartCabinet™ across Europe, Middle East and Africa (EMEA). The Vertiv SmartCabinet is an innovative approach to deploying micro data centres with a complete IT infrastructure solution in a fully-integrated enclosure. Packaged in one simple, intelligent system, this plug and play unit comprises thermal management, power distribution, remote monitoring, infrastructure management and high efficiency Liebert® uninterruptible power supply (UPS).

“Micro data centres at the edge of the network are critical to many businesses, but building and equipping facilities fast enough to meet growing data demands has become an issue,” said Appal Chintapalli, vice president of integrated rack systems for Vertiv in EMEA. “The fully integrated SmartCabinet – which combines all of the necessities for a micro data centre into one single unit – eliminates the need to build complex computer rooms while enhancing system deployment. This enclosure is a must-have for micro data centres with limited space, but also for companies looking to quickly upgrade their server rooms and local nodes to support increased data processing for content delivery, such as mobile computing and the Internet of Things.”

SmartCabinet is pre-engineered, pre-configured and factory tested to ensure system compatibility along with the utmost efficiency and reliability. Ready to use from day one, its compact design means that no dedicated IT room is required. SmartCabinet is designed for a broad range of applications, such as telecommunication sites, retail stores and branch offices, as well as businesses across all sectors, including educational institutions, healthcare, finance, government, transportation and business process outsourcing firms.

Vertiv will be showcasing the SmartCabinet at CeBIT, the global event for digital business, from March 20 to 24 in Hannover, Germany. Stop by Hall 12, Stand D79 to see it first-hand and discuss the infrastructure and edge solutions available from Vertiv. For more information on SmartCabinet, visit www.VertivCo.com/SmartCabinet.

About Vertiv
Vertiv designs, builds and services critical infrastructure that enables vital applications for data centres, communication networks and commercial and industrial facilities. Formerly Emerson Network Power, Vertiv supports today’s growing mobile and cloud computing markets with a portfolio of power, thermal and infrastructure management solutions including the ASCO®, Chloride®, Liebert®, NetSure™ and Trellis™ brands. Sales in fiscal 2016 were $4.4 billion. For more information, visit VertivCo.com.

MEDIA CONTACT
Lara Bunston
T +44 208 618 2821
E Lara.Bunston@fhflondon.co.uk 

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location