Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Saves Water with Single Cabinet based Large DX Solution

As the world becomes more and more digitized, there is an increasing reliance on data centers and computing power to operate the growing digital economy. In storing massive amounts of data, data centers generate a large amount of heat, which has traditionally been dispersed by using water. As a result, data centers are commonly located in areas where both power and water supply are plentiful and cheap. This greatly narrows the range of suitable locations and puts more strain on water usage effectiveness.

Further, there has been a lot of debates on the ideal airflow configuration in the data center. Recently there is another angle to explore to maintain uniform airflow i.e., horizontal airflow configuration. Many colocation & hyper-scale data centers are opting for this configuration by using a massive wall of fans to push the cool air onto the data center floor. The following are the advantages of horizontal airflow configuration:

  • Ideal for non-raised floor critical infrastructure installations with hot aisle containment
  • High adaptability to IT load conditions due to horizontal air flow configuration and variable speed fans

Along with availability, reliability, and energy efficiency white space management is another key in the pursuit of uptime in mission-critical solutions. The ability to tailor an engineered solution is what sets Vertiv apart from other companies.

Vertiv unveils largest & single cabinet-based (all-in-one) DX solution i.e. Liebert PKDX, an engineered Direct Expansion (DX) Package Solution that supports “zero” water-based configuration, increases white space in data center and comes with plug-n-play arrangement, eliminates underfloor arrangement, and increases resultant PUE and “ZERO WUE”.  Liebert PKDX with ZERO WUE for cooling will bring a new paradigm for the development of green and low carbon emission technologies. Liebert PKDX is also available in Split version.

 

 

Features Benefits
  • Single cabinet solution
  • Zero footprint in data hall
  • Equipped with Digital and tandem compressor configuration
  • Higher Air volume
  • Higher return air temp
  • 300kW capacity/Unit
  • Intelligent Control
  • Hot Aisle Containment
  • Quick and easy deployment
  • More white space available for IT equipment
  • Improved variable load efficiency
  • More racks served in a single unit
  • Enhanced pPUE
  • Reduced number of cooling units required
  • Plug-and-play configuration
  • Optimized thermal management

 

Application:

Customer Type Application Challenges Solution

Colocation and Cloud

Medium-Large Critical Space Non-raised Floor High-Capacity Single Unit, White Space Limitation

Vertiv™ Liebert® PKDX is designed for critical applications such as data center, control rooms without a raised floor. A single cabinet- based DX unit of 300 kW consists of an evaporator and condenser section that can handle very high air volume up to 74700 CMH and high ESP up to 300 Pa. Liebert® PKDX doesn’t occupy white space in the data hall/control room.

Financial Institution

Medium-Large Critical Space Space Limitation, Non-raised Floor

Telecom Sector

Large Switch Room, Data Center, Critical Space Non-raised Floor, High- Capacity Single Unit, White Space Limitation

Icons.jpg

In 2023, Vertiv India has unveiled the availability of the Liebert PKDX in Greater India and Southeast Asian countries. To learn more, click here.

PRODUCTS & SERVICES
Overview
PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location