Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Immersion cooling systems: Advantages and deployment strategies for AI and HPC data centers

7 min. Read

Data center infrastructure is rapidly expanding, fueled by the ongoing rise of artificial intelligence (AI) and high-performance computing (HPC) workloads. As rack densities continue to increase, operators evaluate their liquid cooling strategies and plan for future capacities of up to 600 kilowatts (kW) per rack and beyond.

Rear door heat exchangers (RDHxs) and direct-to-chip cooling manage current heat levels. However, the persistent densification suggests more advanced cooling solutions. Data center immersion cooling (or “liquid immersion cooling”) is an energy-efficient option that provides superior cooling for high-density workloads.

Learn more:

Data center operators are evaluating liquid cooling technologies to increase energy efficiency as processing-intensive computing applications grow.

Liquid cooling options for data centers

  

Understanding immersion cooling

Immersion cooling (see Figure 1) involves submerging servers and other rack components in a thermally conductive dielectric liquid or fluid inside a sealed tank. The fluid efficiently absorbs heat from IT equipment, providing excellent cooling for high-performance computing workloads.Vertiv™ CoolCenter Immersion Cooling Tank

Figure 1. Vertiv™ CoolCenter Immersion is an example of an immersion cooling tank. The IT equipment is placed horizontally in a sealed tank resembling a server rack on its back, following a typical 19-inch standard. Servers are inserted from the top and positioned vertically.

The absorbed heat is pumped to a coolant distribution unit (CDU) with a a brazed plate heat exchanger. A primary cooling loop, linked to a chiller, dry cooler, or waste heat recovery system, is separated from the secondary loop holding the dielectric liquid. This setup efficiently moves heat out of the building.

Components of immersion cooling systems

Data center immersion cooling relies on several critical components for effective deployment:

  • Tank: Sealed containers that hold IT equipment and dielectric fluid, equipped with sensors, a power distribution unit (PDU), and other monitoring systems.
  • CDU (see Figure 2): Circulates and pumps coolant in a closed-loop system between the tank and the chilled water supply. These units include the following components:
    • Heat exchanger -
    • Transfers heat from the dielectric fluid to the building’s chilled water without mixing fluids.
    • Pumps - Circulate the liquid into the tank around the servers, removing heat from the IT components and heating up the fluid. The liquid is then pumped to the brazed plate heat exchanger to cool down before passing through a filter and returning to the tank to start the cycle again.
    • Flow modulating valve - Adjusts the cooling capacity of the CDU to match the heat load within the tanks, enabling optimal thermal management and efficiency.
    • Filter - Removes contaminants and impurities from fluids to maintain optimal operation and longevity of systems.
    • Power supply - Enables seamless power transition with an integrated AB transfer switch.
  • Piping: Connects the tank to the CDU to facilitate the circulation of the dielectric liquid.

Vertiv™ CoolCenter CDU

Figure 2. The Vertiv™ CoolCenter Immersion CDU manages and distributes chilled liquid to immersion cooling systems, efficiently removing heat from submerged data center equipment.

Efficiency and performance of immersion cooling
for HPC

Immersion cooling can enhance data center performance by efficiently managing high heat outputs. In AI and HPC workloads, immersion cooling systems have delivered cooling capacities of up to 100 kW per tank (42 or 52 rack units (U)). This technology can provide an effective solution for intense computational demands.

Cooling capacity of immersion systems

Immersion cooling absorbs 100% of the heat from IT components since they are fully submerged in the fluid, minimizing the need for air cooling units and reducing heat transfer steps. This system’s capacity to handle all heat from components eliminates residual heat in the air. Moreover, the fluid used in immersion cooling operates at higher temperatures than direct-to-chip cooling, allowing longer free cooling periods. When using a chiller, the smaller temperature difference can improve energy efficiency.

However, room cooling units will remain essential in a data center to maintain air quality. Controlling humidity and using a filtration system can prevent dust build-up, facilitate clean air circulation, and maintain breathable conditions by reducing excess CO2.

Environmental impact

Immersion cooling systems often use a mineral-based dielectric liquid from natural gas. Natural gas can be used as a source material to create a dielectric fluid through the "gas-to-liquids" process, where it is converted into a synthetic liquid suitable for immersion cooling applications. Although the chemical industry purifies and converts this oil into a new dielectric liquid, this prevents CO2 emissions. The immersion cooling liquid is not consumed, as is the case with natural gas in electrical power plants.

Data center operators aiming for an oil and natural gas-free immersion cooling liquid can use bio-based dielectric liquids as an alternative. These liquids, derived from biological waste, reduce reliance on mineral oil and natural gas, offering a more environmentally conscious option.

Unexpected benefits

Immersion cooling can offer a quieter data center environment. Unlike the noise prevalent in air-cooled centers—due to extensive air recirculation—immersion cooling is predominantly silent, with only the soft hum of pumps, significantly reducing overall noise levels.

Learn more:

Vertiv™ AI Hub:

Vertiv™ 360AI includes a complete portfolio of power, cooling and service solutions that solve the complex challenges arising from the AI revolution.

Critical considerations for retrofitting with immersion cooling systems

Not all data centers requiring liquid cooling solutions are greenfield installations. When retrofitting an existing air-cooled data center with immersion cooling, key considerations for operators include space layout and power infrastructure.

Space and layout

Immersion tanks have a different footprint compared to traditional racks, so immersion cooling systems don't fit a standard data center layout with racks. To deploy immersion tanks effectively, facility teams can assess available space and plan accordingly, possibly reconfiguring layouts to accommodate the required space. Before operations begin, they must clear a designated zone for tank and CDU implementation.

Power infrastructure

Immersion cooling systems need a direct power supply, requiring facility teams to reconfigure their power infrastructure. Data center operators can use an A and B feed with a UPS backup and connect CDUs to a power source similar to the IT equipment. This allows CDUs to stay operational with the IT systems and provide cooling even during a power outage.

Customizing immersion cooling systems

Immersion cooling can be tailored to meet the unique requirements of different data centers by addressing specific needs such as network components and PDU. For instance, some setups require more space for network switches beyond the standard 2U compartment, while others need customized PDUs for higher power output, more outlets, or alternative configurations. Liquid flow rate adjustments are also feasible, but the primary customizations often involve network and PDU setups.

Scalability of immersion cooling

Data center operators can efficiently scale their immersion cooling deployments to accommodate future growth. Each CDU provides a cooling capacity of 200 to 240 kW, allowing data centers to scale in 240 kW increments. With this design, operators can add one to four tanks per CDU, with each tank supporting up to 100 kW. Therefore, to achieve the full 240 kW capacity, multiple tanks would be required. This modular approach suits large data centers with high-density server deployments, allowing for precise scaling according to demand.

Best practices for immersion cooling deployments

The monitoring requirements for immersion cooling systems differ slightly from those of traditional air-cooled data centers. Most operators might already know about some parameters, such as temperature and pump seeds, as these are also used in CDUs for direct-to-chip cooling.

However, immersion systems introduce new data points, such as multiple tank levels requiring unique alarm setups. These alarms are categorized as urgent or non-urgent, similar to air-cooled system alerts for server room door status. Existing building management systems (BMS) can easily integrate these additional data points, such as fill levels and tank temperatures, into their frameworks. Although the specific data points might have different names, the fundamental features and integration processes align closely with those of conventional systems.

Learn more:

Create a roadmap for liquid cooling
installation by downloading our guide:

Deploying liquid cooling in the data center

Liquid cooling services for immersion systems

Immersion cooling systems require consistent and expert services to maintain uninterrupted performance, supporting the reliability and scalability of high-density AI and HPC workloads. Vertiv’s liquid cooling services by optimize power usage, enhance efficiency, and enable seamless operations for high-density AI applications. With end-to-end lifecycle support, global expertise, and certified technicians, we provide scalable, AI-ready solutions that maximize performance and minimize risk. 

  • Startup and commissioning services: We provide precision installation support, full system testing, and seamless transition to operation, keeping your liquid cooling system ready for high-density AI workloads.  
  • Fluid maintenance and analyses: Our services include coolant sampling, quality testing, and chemical adjustments to maintain system integrity and prevent issues like blockages or corrosion.  
  • Ongoing maintenance and support: Regular inspections, fluid management, and proactive upgrades keep your liquid cooling systems efficient, reliable, and compliant with industry standards.  
  • Spare parts: With a global network of field engineers and readily available spare parts, we facilitate quick repairs and minimal downtime for continuous operations.  
  • Digital services: Leveraging AI-driven data analysis, we offer remote troubleshooting, condition-based maintenance, and anomaly resolution to optimize system performance.  
  • Vertiv-certified technical support: Our certified technicians provide expert site assessments, installations, and maintenance, allowing your liquid cooling systems to operate at peak efficiency.

Learn more:

Liquid cooling services

As heat surges in high-performance computing environments, the need for liquid cooling technologies in modern IT thermal management becomes critical.

Emerging trends and prospects in immersion cooling

The future of immersion cooling is advancing with increased cooling capacity. We’ll likely see a combination of liquid cooling solutions, including various innovative methods integrated into specialized systems.

Another significant trend is the improvement of dielectric liquids, providing alternatives that help reduce carbon emissions. Moreover, immersion cooling allows for increased cooling system temperatures, which enhances waste heat recovery processes. This progress opens opportunities for district heating applications and other uses.

Choose your path to high density

Your journey to high-density can be a smooth ride. Vertiv designs advanced solutions to power and cool the most challenging deployments. Unleash your AI Evolution with Vertiv today.


Blog Posts Thermal chain evolution (about) Thermal Management Trends
PARTNERS
PARTNERS
Partner Login

Language & Location