Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

eStruxture Scales to Meet Colo Customer Needs with Wall-to-Wall Vertiv Solutions

 

 

When transforming a former printing press facility into a state-of-the-art data center, eStruxture wanted to give companies the ability to design multi-site, carrier- or cloud-neutral data center solutions with the scale and flexibility to accommodate any workload or power density requirement.

Background

At the time of eStruxture’s founding in April 2017, the company realized that its customers lacked choice when it came to cloud- and carrier-neutral colocation and connectivity solutions. The company founder, who spent many years in the telecom industry, realized that the existing carriers and smaller providers either lacked a pan-Canadian presence or the capital to invest in meeting customers’ growing and evolving requirements — needs he could meet with Vertiv as a partner.

Results

  • Optimized use of computing space that allows for additional customer offerings such as dedicated halls with office space, storage, and disaster recovery options
  • Ability to support customers with high-density requirements by offering up to double the capacity of most competitors with 30 kW per rack standard
  • New facility ready for turnover six months earlier than previous builds
      
Case Summary
Location:

MTL-2 data center in Montreal, Canada

Critical Need:

When transforming a former printing press facility into a state-of-the-art data center, eStruxture wanted to give companies the ability to design multi-site, carrier- or cloud-neutral data center solutions with the scale and flexibility to accommodate any workload or power density requirement.

Vertiv Solution:
  • Liebert® EXL S1 UPS units with lithium-ion batteries (LIB) installed in parallel 2+1
  • Liebert® DSE free-cooling economization system with Liebert® iCOM™ controls
  • Liebert® PPC power conditioning and distribution cabinet with branch monitoring
  • Liebert® RX distribution cabinet with branch monitoring
  • Vertiv™ VR racks with Vertiv Geist™ rack power distribution units (rPDUs)

DOWNLOAD THE CASE STUDY

 

PARTNERS
PARTNERS
Partner Login

Language & Location