Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Optimized for AI: EdgeConneX’s data centers leverage Vertiv’s advanced power technology

25/3/25

EdgeConneX  cooperated with Vertiv to rigorously test the performance of large UPS systems under the extreme power demands of AI variable loads. The tests, conducted on the Vertiv™ EXL S1 UPS—designed with the same advanced architecture of Vertiv™ Trinergy™—confirmed that the UPS provides reliable power continuity and energy efficiency, meeting the rigorous needs of AI-driven data centers. This partnership highlights how Vertiv’s innovative power technologies enable EdgeConneX to transform its vision of AI-powered data centers into reality, driving digital intelligence and delivering value across industries globally. 

Background:

As AI adoption accelerates, data centers face unprecedented challenges in managing higher and more dynamic power demands. EdgeConneX, a global data center provider, partnered with Vertiv, a global leader in critical infrastructure technologies to validate the performance of Vertiv™ EXL S1 UPS, Vertiv's large UPS system that shares component architecture with the recently launched Vertiv™ Trinergy™, to see how the systems perform under AI variable loads. The results demonstrated that Vertiv’s UPS solutions provide reliable power continuity and energy efficiency, enabling the resilience and performance required for AI-driven data centers. 

Results:

  • Stable output regulation: The Vertiv™ EXL S1 UPS maintained stable output voltage and current during high compute and idle cycles of AI training, maintaining consistent power delivery despite rapid fluctuations in load. 
  • Seamless power transition: The Vertiv™ EXL S1 UPS demonstrated seamless transitions between utility power and generator power, effectively managing the switch without any interruptions or power quality issues, which is critical for maintaining AI application performance. 
  • Overload capabilities: The UPS system managed overload conditions supporting the intensive processing tasks of AI without any degradation in performance. 
Case Summary
​Location:​

Atlanta, USA  

Critical Need:

AI variable loads present significant challenges for data centers, including rapid power fluctuations, sustained high energy demands and the need for seamless transitions between power sources. Traditional infrastructure often struggles to keep up, leading to inefficiencies and potential disruptions. To overcome these challenges, EdgeConneX collaborated with Vertiv to rigorously validate its Vertiv™ UPS systems, proving they can reliably handle the intense and unpredictable energy requirements of AI variable loads. 

Through Vertiv’s advanced power solutions, EdgeConneX successfully developed AI-optimized data centers, ready to support the next wave of digital innovation. This collaboration underscores the critical importance of resilient power infrastructure in driving the future of AI-powered computing. 

Vertiv Solution:

DOWNLOAD THE CASE STUDY

Watch the video: AI and the future of data centers | EdgeConneX meets Vertiv to talk about the AI Factory

 

PARTNERS
PARTNERS
Partner Login

Language & Location