Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces New Prefabricated Modular Data Center Solution to Allow Large Capacity Expansion for Customers in Latin America

March 27, 2023

Vertiv™ MegaMod™ and Vertiv™ MegaMod™ Plus are standardized data center modules that cut deployment time by up to 30% compared to traditional construction.

Argentina [March 27, 2023] - Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ MegaMod™ and Vertiv™ MegaMod™ Plus, a turnkey prefabricated modular (PFM) data center solution, deployable in expandable units of 0.5 or 1 megawatts for IT loads up to 2 megawatts or more. The high-quality prefabricated modules are integrated and tested with industry leading Vertiv™ power management systems, thermal management solutions, remote monitoring and IT equipment racks to deliver exceptional performance and help companies reduce deployment time by up to 30% compared to a traditional data center build. The solutions are now available across Europe, the Middle East and Africa (EMEA), and Latin America. 

Companies are racing to deploy processing power in new locations to meet the demand for digital business products and services. The MegaMod™, and the MegaMod™ Plus, which offer up to 25% more rack and cooling capacity, enable customers to expand core-to-edge data center networks and to rapidly deploy new compute capacity with lower upfront costs, greater predictability and less risk than traditional data center builds, thanks to proven industrial processes and high standards of quality control. Both solutions provide options to grow horizontally or vertically, with MegaMod™ providing cooling capacity in the IT Hall area, while MegaMod™ Plus is configured with cooling modules that support the IT Hall space expansions.  

“The Latin American region has witnessed a boost in the modular data center market due to factors such as deployment of edge data centers, sustainability measures in the data center market, or the growing demand for big data and IoT. But at the same time, data center owners and operators must sort multiple challenges such as supply chain issues, talent gap or location constraint when building and bringing white space data centers online. Either way, Vertiv prebuilt MegaMod™, can be used to overcome these challenges, while providing plug-and-play data center capability where and when it's needed,” said Alexandre Alves, Integrated Solutions Offering Manager for Vertiv LATAM. 

The flexible solution capacity is ideal for medium size data centers and can be easily deployed and expanded if the business needs to grow. Vertiv also provides end-to-end services for a straightforward start-up and smooth operations, including deployment, commissioning, ongoing maintenance, remote monitoring and training. 

For more information on the MegaMod™ and other data centers solutions from Vertiv, visit Vertiv.com or contact your local Vertiv representative. 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise. 

CONTACT

Ivis Cruz Fernandez
T +1 305-3355883
ivis@ivicomm.com 

PARTNERS
Partner Login

Language & Location