Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Introduces New Single-Phase Uninterruptible Power Supply for Distributed IT Networks and Edge Computing Applications in Latin America

May 11, 2023

New Vertiv™ Liebert® GXE UPS is a high-performance and cost-effective solution delivering secure and efficient power protection

Santiago, Chile [May 11th, 2023] - Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today introduced the Vertiv™ Liebert® GXE, an online double-conversion single-phase uninterruptible power supply (UPS) available in 6 and 10 kVA power ratings in tower or rackmount configuration. The system is designed to provide reliable power to distributed IT networks and edge computing applications in various industry segments such as enterprise, government, manufacturing, finance, education and retail. ​The product is globally available for countries and organizations using 230V solutions and is now shipping from stock in Latin America, Europe, Middle East and Africa (EMEA).

The Liebert® GXE performs with high efficiency up to 94% in online mode and up to 98% in ECO mode, driving energy and operational costs savings compared to other models available on the market. The high output power factor of 1.0 enables continuous and reliable power to more connected devices, protecting them against many disturbances in the AC mains with the online double conversion technology and the input surge protection.​ The flexible rackmount or tower form factor, with rackmount kits included as a standard, facilitates stock management for distribution in the IT channel and simplifies installation to accommodate various micro data center and edge computing needs.

The unit’s runtime can be extended with up to four external battery cabinets (EBC) for longer back-up protection, and the hot-swappable VRLA batteries can be easily replaced by users without the assistance of skilled personnel and without shutdown of the loads for smoother operations and minimized maintenance costs. Additionally, the Liebert GXE has an integrated 4 Amps charger providing quick battery recharge up to 90% in just 3 hours that can be critical in case of frequent mains failures, and an integrated battery management system to optimize battery life and recycling.

The Vertiv™ Liebert® GXE includes a user-friendly LCD color display that makes it easy and intuitive to use. The unit offers remote monitoring capabilities for quick and easy access to IT infrastructure, through the optional Vertiv™ Liebert® Intellislot™ Unity Communications card and a free download of Vertiv™ Power Insight software. Moreover, customers can also rely on Vertiv™ LIFE™ Services to support remote maintenance and servicing of the UPS for maximum availability.

“Distributed and edge data centers today are no less critical to business success than large centralized data centers, given their role in supporting the Internet of Things, cloud computing and other crucial applications. This unit helps to protect mission critical equipment in the event of power loss or power fluctuations in a multiple market segments in LATAM,” said Rodrigo Lopez, IRS offering lead, Vertiv LATAM.

Vertiv channel partners can take advantage of a complete range of warranty extensions and service programs specifically designed for single-phase UPS systems, which can be renewed so as to cover the entire lifecycle of the product. Vertiv service programs are available in a selection of countries, check Vertiv.com for specific country availability or contact your local representative.

For more information about Vertiv and its channel portfolio, visit Vertiv.com. Click on “Partners” and “Apply Now” to take full advantage of what Vertiv has to offer.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT
Ivis Fernandez
T +3053355883
E ivis@ivicomm.com

PARTNERS
Partner Login

Language & Location