Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv’s External Lithium-Ion Battery Allows Conversion of Existing VRLA-Based UPS to Lithium-Ion Backup at the Network Edge in LATAM

July 24, 2023

Vertiv™ MPL Lithium-Ion Battery provides the benefits of lithium-ion to Vertiv™ Liebert® ITA2 uninterruptible power supply systems, bolsters Vertiv’s lithium-ion product portfolio

Columbus, Ohio [July 17, 2023] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced the release of its Vertiv™ MPL Lithium-Ion Battery, an external battery that allows the user to convert their existing VRLA-based Vertiv™ uninterruptible power supply (UPS) system to a lithiuim-ion system. The Vertiv MPL Lithium-Ion Battery is currently compatible with installed Liebert® ITA2 UPS systems using valve regulated lead acid (VRLA) batteries, providing the benefits of lithium-ion without the need to replace the UPS. The Vertiv MPL Lithiuim-Ion Battery is available in 208V versions in Dominican Republic, Puerto Rico, Costa Rica, El Salvador, Guatemala, Honduras, Nicaragua, Panama, Mexico, Colombia, Ecuador and Venezuela.

Compared to VRLA batteries, the Vertiv MPL Lithium-Ion Battery has a life up to three times longer, reducing costs related to replacements and maintenance and offering a lower total cost of ownership. Less than half the size and weight of VRLA equivalents, the lithium-ion option is ideal for small spaces, with 1U and 2U sizes that provide the runtime capabilities and reliability needed for most standard edge applications. Up to eight batteries may be added to each supported Vertiv™ UPS, with battery run-time based on system capacity, connected load and number of battery modules.

 A local Vertiv™ Services representative will make the physical and firmware changes that allow the UPS to operate with the Vertiv MPL Lithium-Ion battery. This representative will also install the batteries in rackmount or tower configuration and remove and dispose of the VRLA battery that previously supported the UPS. Optional startup service is also available. The Vertiv MPL is covered by a limited 5-year warranty.

"From now on, customers can implement the Vertiv™ Liebert® ITA2 UPS with lithium-ion batteries, while previously these UPS systems were limited to VRLA batteries. We are offering this option so customers can move to lithium-ion battery technology without needing to reinvest or completely replace their UPS installation”. For all those interested in implementing our new lithium-ion solutions, contact Vertiv to discuss how to upgrade your current or new installation, explained Vertiv's integrated rack systems offering lead, Rodrigo López.

The Liebert® ITA2 UPS is an energy-efficient 3-phase UPS in 8 and 10kVA capacities, suitable for network edge and other IT applications. 

For additional information, visit Vertiv.com.

 

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to enable its customers’ vital applications to run continuously, perform optimally and grow with their business needs. Vertiv solves the most important challenges facing today’s data centers, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Westerville, Ohio, USA, Vertiv does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

 

Forward-Looking Statements

This release contains forward-looking statements within the meaning of the Private Securities Litigation Reform Act of 1995, Section 27 of the Securities Act, and Section 21E of the Securities Exchange Act. These statements are only a prediction. Actual events or results may differ materially from those in the forward-looking statements set forth herein. Readers are referred to Vertiv’s filings with the Securities and Exchange Commission, including its most recent Annual Report on Form 10-K and any subsequent Quarterly Reports on Form 10-Q for a discussion of these and other important risk factors concerning Vertiv and its operations. Vertiv is under no obligation to, and expressly disclaims any obligation to, update or alter its forward-looking statements, whether as a result of new information, future events or otherwise.

 

CONTACT

Sara Steindorf
T +314-982-1725
sara.steindorf@fleishman.com

PARTNERS
Partner Login

Language & Location