Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Clariden Bank Chooses Avocent® Data Center Management Solutions from Vertiv

12/20/18

Background

Complete control over both data centers is important to the system administrators, and not just during working hours. Access during standby service periods is also possible on the basis of a variety of encryption mechanisms and access controls. Clariden Bank chose the DSR™ 2010 KVM over IP switch from Avocent because the solution enables servers to be controlled and managed from any administrator workplace via standard IP connections within a shielded network, regardless of distance.

Results

  • The digital server management solution developed by Avocent meets the highest demands in the sensitive area of data protection at this bank. All systems protected by a firewall are managed using the Avocent DSR switching solution.
  • Both locations have sufficient resources to monitor business critical data and applications. Using the Avocent DSView® software interface, the system administrator can monitor the status of all computers.

Case Summary
Location:​

Zürich, Switzerland

Critical Need: Complete control over both data centers is critical. The digital server management solution must meet the highest demands in the sensitive area of data protection.
Vertiv Solution:
  • Avocent DSR 2010 KVM over IP switch
  • Avocent DSView software interface
Download the Case Study

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview

Language & Location