Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Deltalis

11/22/17


Deep in the Swiss mountains, in a former military bunker, there is a company providing modular and scalable data centre services. From pure housing through to full managed services - with an extraordinary level of security - DELTALIS is quite unique. In addition to physical security, this location frees the facility from the risks associated with an urban environment such as vibrations, overloaded energy networks, civil works and construction. And yet, being located only 60 minutes from Zurich, it’s connected to one of Europe’s thriving commercial hubs, ideal for both domestic and international accessibility.

Case Summary
Location:

Zurich, Switzerland

Critical Need: To deliver absolute physical and digital security so that the clients could trust Deltalis without question. Deltalis also wanted to provide a facility that would be trusted within the Swiss market - one of the most demanding anywhere globally. Finally, the aim was to offer customised services, delivering a more bespoke experience than can be found elsewhere in the market.
Vertiv Solution:
  • Trellis Inventory Manager for capacity management and change management which supports ISO 27001 compliance
  • Trellis Power Systems Manager to control and manage power consumption and efficiency
  • Trellis Site Manager to get a centralised view on the facility and centralise alarms to ensure compliance to ISO 27001
Download the Case Study
PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview

Language & Location