Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Pumped Refrigerant Economization Eliminates California Data Center Water Usage

That’s the amount of water that can be eliminated annually in a 1MW California data center by using pumped refrigerant economization, compared to water economization.

The California Energy Commission in 2015 approved using the Liebert DSE system freecooling with pumped refrigerant economizer in the state’s data centers, as part of its prescribed economization methods under Title 24. Previously, the Commission’s prescribed usage included only air and water economizers.

Higher Efficiency Without Using A Drop

The Liebert DSE freecooling system with pumped refrigerant economizer maximizes annual economization hours – and uses no water. With this system, data centers in California can:

  • Cut annual water usage by 4.3 million gallons for a typical 1MW data center
  • Reduce Time Dependent Value of energy by 8 percent to 10 percent
  • Eliminate water treatment costs and hazards
  • Eliminate the risk of outside air contamination
  • Maximize protection and efficiency through integrated advanced controls

Vertiv has published a full report showing the analysis of pumped refrigerant economization compared to water-side and air-side economization.

Read the Report

Related Articles

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview

Language & Location