Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Line-Interactive UPS Systems

Cost-Efficient, High Performance Network Power Protection

Line-interactive uninterruptible power supply (UPS) systems provide both power conditioning and battery backup. This technology is particularly effective in areas where outages are rare, but power fluctuations are common. Line-interactive UPS systems support a wide range of input voltage fluctuations before switching to battery backup.

Line-interactive UPS technology provides power conditioning with a 4-6 millisecond break in power when transferring to battery back-up and protects against the most common power problems experienced in a network. Here the UPS also monitors the voltage level and balances under and over voltages. This technology provides a good choice between reasonable protection and moderate operating costs.

With line-interactive UPS, the inverter becomes part of the output and is always on. The inverter can operate in reverse to charge the battery while AC input is normal and switch to battery power when input fails. Internal components provide filtering and voltage regulation that raises and lowers utility power to the level needed by the connected equipment. In some cases, line-interactive UPS systems rely on the battery to condition power so it may use the battery more frequently than online UPS systems that condition power through the double-conversion process.

When AC input power fails, the unit’s transfer switch opens and the power flows from the battery to the UPS output. With the inverter always on and connected to the output, line-interactive UPS provides additional filtering and yields reduced switching transients when compared to a standby UPS. Line-interactive UPS systems are typically used in rackmount applications below 5000VA.

Featured Products

With capacities ranging from 800VA to 5000 VA, the Liebert PSI5 is a compact rackmount or tower, Automatic Voltage Regulation (AVR) line-interactive UPS system designed especially for IT applications such as network closets and small data centers. The Liebert PSI5 UPS supports advanced pure sine wave output on battery to safeguard critical IT equipment and business electronics. It provides reliable power protection for servers, critical nodes, network workstations, large network peripherals, network routers, bridges, and other electronic equipment.

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview

Language & Location