30% is the amount of time that cooling units will conflict with each other without data center cooling unit coordination. One unit will cool, while another is reheating, resulting in wasted energy.

Intelligent controls can solve this problem. They use machine-to-machine communications and advanced algorithms to coordinate unit operations, balancing airflow, air temperature and humidification. That reduces conflicts and saves money.

Intelligent Liebert® iCOM Unit Controls Coordinate Multiple Cooling Units to Save Money

Eliminating reheat by a single cooling unit in conflict with another cooling unit can cut the number of reheat hours by approximately 30 percent, providing significant energy savings.

Terms of Use.  All comments are moderated by Vertiv Co.  Comments that in the sole discretion of Vertiv Co. violate these terms or are deemed to be offensive in nature are subject to removal. By registering you acknowledge acceptance of these terms


There are no comments. Be the first one to write one.


SUPPORT
ABOUT
Overview
News & Insights

Language & Location