Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Analysis of Pumped Refrigerant Economizers

November 15, 2016

The California Energy Commission has approved the Liebert EconoPhase Pumped Refrigerant Economizer used by the Liebert DSE thermal management system for use in California data centers under The California Energy Code (Title 24), as an alternative prescriptive method.

The California Energy Code (Title 24) requires data centers to meet the efficiency requirement of one of three economization methods (outside air economization, water economization or pumped refrigerant economization) or to demonstrate that a proposed solution meets or exceeds the energy efficiency of the prescriptive methods. This paper describes the data, calculations and modeling that led to approval for pumped refrigeration as an option for data center cooling.

Key Takeaways

  • The use of refrigerant economizers provides significant benefits in California data centers — there is on average a 5% to 6% reduction in the TDV (Time Dependent Valuation) energy value, but more significantly it eliminates the water requirement for these data centers.
  • The inclusion of a refrigerant economizer, such as the Liebert® DSE™ system with Liebert EconoPhase™ pumped refrigerant economizer, in the prescriptive compliance method makes the adaption and implementation of this technology on par with water economization evaluations.
  • The Liebert DSE data center cooling system with pumped refrigerant economization system is a break-through technology that solves many building design issues for thermal management needs, and meets or exceeds the efficiency of most water and air economization methods.

Download the White Paper

Related Articles

PARTNERS
Overview
Consultants Corner
Partner Login

Language & Location