Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

AI infrastructure at scale and
built multiple generations ahead

Vertiv solutions underpin hyperscale and cloud facilities that
define today and make tomorrow possible

The proliferation of AI and relentless, explosive demand for cloud computing is forcing a sudden reimagining of the industry’s innovation laboratories

Unlocking the potential of AI

AI is already changing the way we work, learn and innovate, and we’re just scratching the surface of what’s possible. Finding its limits means reimagining how we power and cool hyperscale facilities.

Managing energy consumption and costs

Average rack densities will reach 50 kW by 2027, and many AI servers are soaring past that number today. Powering those racks without overextending the grid or the bottom line requires new thinking about non-traditional energy sources and power architectures.

Scaling with speed to meet demand

Meeting unrelenting demand for AI and other advanced applications means adding capacity quickly and efficiently while eliminating waste and costly delays. The ability to grow when, where and how it’s needed separates the winners from the rest.

Find your hyperscale and cloud solution

Holistic AI infrastructure

 

Support the full spectrum of AI workloads and simplify your AI upgrade with integrated, pre-engineered solutions

Power management across the entire power train

 

Rapidly scale to meet growing power demand

Full spectrum of high-density cooling solutions

 

Solutions that can be configured as air, liquid or hybrid cooling and field-converted to meet your needs

The Vertiv advantage

Vertiv solves the most demanding, complex challenges facing today’s cloud providers with the industry’s broadest, most diverse portfolio of leading-edge hyperscale infrastructure solutions.

more energy efficient1

based on close technology
faster deployment times2

TCO savings3

1. Up to 20% lower annual cooling energy consumption with Vertiv™ Liebert® AFC chillers, compared to traditional fixed screw solutions

2. Up to 50% faster deployment with Vertiv MegaMod compared to onsite build

3. Comparison between module vs. traditional stick built. Percentages based upon management estimates, case studies and publicly available data.

Vertiv™ OneCore

Rethink the roadmap for AI adoption

Supporting increasing demand for AI requires new approaches to hyperscale infrastructure and operation. This e-book identifies imperatives to help cloud providers and hyperscalers align their infrastructure and operational strategies to meet the demands of AI.

Learn more

Dig deeper

AI imperatives image

Powering the cloud: Is it time to bring your own?

Learn how BYOP can reduce your grid dependence and carbon footprint while optimizing operational efficiency.

Explore

chilled water solutions image

Data center vision 2030: How AI is redefining data center infrastructure

Explore how AI and accelerated compute is shaping the key power, cooling and services to support AI workloads and infrastructure.

Explore

Colocation whitepaper image

Always-on energy: Integrating a BESS into your microgrid strategy

Learn how to use a battery energy storage system and microgrid as an always-on energy source and supplemental revenue stream.

Get the white paper

Need help selecting a hyperscale and cloud solution?

Please fill out the form below and we will get back to you as soon as possible.

PARTNERS
Overview
Consultants Corner
PARTNERS
Overview
Consultants Corner
MY ACCOUNT
Overview

Language & Location