Al trabajar con el soporte de ventas de Vertiv, puede configurar los complejos diseños de acuerdo con sus necesidades específicas. Si forma parte de una organización que busca orientación técnica para un proyecto grande, Vertiv puede ofrecerle el soporte que necesita.

Más información

Muchos clientes trabajan con un socio revendedor de Vertiv para comprar productos de Vertiv para sus aplicaciones de TI. Los socios cuentan con amplia capacitación y experiencia, y están en una posición única para especificar, vender y brindar soporte a soluciones completas de TI e infraestructura con los productos de Vertiv.

Buscar un revendedor

¿Ya sabe lo que necesita? ¿Desea la comodidad de comprar y enviar en línea? Ciertas categorías de productos de Vertiv se pueden comprar a través de un revendedor en línea.


Encontrar un vendedor en línea

¿Necesita ayuda para elegir un producto? Hable con un especialista de Vertiv altamente calificado, quien le guiará hacia la solución adecuada para usted.



Contactar a un especialista de Vertiv

Insurance Leader Integrates Legacy Platforms with Environet for Core-to-Edge Visibility and Control

20/3/19

One of the largest non-public companies in Ohio implemented the Vertiv Environet monitoring system as a way to integrate multi-vendor, legacy equipment that utilized varied communication protocols while gaining improved visibility and control of its network facilities, resulting in improved uptime, efficiency, safety, and overall asset management.


Background

When first evaluating data center infrastructure management (DCIM) systems for a primary data center and 25 edge locations, this leader in personal and commercial lines of property-casualty insurance needed a vendor-neutral solution that could communicate to multiple protocols such as BACnet, Modbus and TCP/IP. The company, formed by community leaders seeking to protect the property of local farmers, also sought a solution that could be integrated with its existing building management system (BMS), and therefore, chose the Vertiv Environet monitoring system.


Results

  • Improved uptime due to immediate notification of issues which enabled fast, local response
  • Increased cooling efficiency through data-supported ROI calculations completed prior to
    infrastructure changes
  • Enhanced first responder safety with the floorplan display that allowed individuals to locate problems without entering a facility
  • Better asset management through evaluation of system data collected from all critical facilities
  • More educated workforce due to a Vertiv relationship which included detailed product training

Case Summary
Location:​

United States

Critical Need:

With continued growth and the need for distributed digital assets, this insurance company wanted improved visibility and control of its portfolio of diverse equipment that used varying communication protocols. Primarily, the company needed a holistic view of its assets for effective management of its network from core to edge.

Vertiv Solution:
  • Vertiv Environet data center monitoring system



DOWNLOAD THE CASE STUDY

Iniciar Sesion Como Socio

Idioma y ubicación