Most administration tasks on the PDU can be done either locally or remotely with the DSView 3 software to provide a real-time view of all connected devices. Using the web interface through the DSView 3 software, the administrator can configure the PDU. Other authorized users can access connected devices for the purposes of troubleshooting, performing maintenance, cycling power and rebooting connected devices.
Figure 1: Unit Overview Screen
| Number | Description |
| 1 | Top option bar. The name of the logged-in user appears on the left side and Bookmark, Refresh, Print, Logout and Help buttons appear on the right. |
| 2 | Tab bar. Only the Units tab applies for the PDU. |
| 3 | Side navigation bar. Menu options are for configuration, viewing of system information and access to devices. The options change based on user type. |
| 4 | Content area. Contents change based on the options selected in the side navigation bar. |