Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Vertiv Continues to Develop Thermal Management Innovation with New Partnership and Chiller Products to Improve Efficiency and Sustainability

maart 11, 2020

Technology partnership with Geoclima and new oil-free centrifugal chiller range delivers technology to enable data centre operators to exceed efficiency targets.

London, UK [March 11, 2020] – Vertiv (NYSE: VRT), a global provider of critical digital infrastructure and continuity solutions, today announced a series of measures designed to meet increasing customer demand for innovative and efficient thermal management technologies and services. This includes Vertiv Liebert® OFC, a new and highly advanced range of oil-free turbocor compressor chillers launched in partnership with Geoclima. The family of air-cooled and water-cooled chillers will initially be available in Europe, Middle East and Africa (EMEA).

The exclusive technology partnership with Geoclima, a company specialising in innovative cooling systems with low environmental impact, enables Vertiv to build on existing world-class chiller technology and a well-established track record around the globe. The Liebert® OFC design has been optimised to utilise low GWP refrigerants including R1234ze and to provide high energy efficiency. Other refrigerants including R513A and R134a are also available in the range.

Kevin Brady, vice president and general manager of Thermal Management for Vertiv in Europe, Middle East and Africa, said: “We believe both Vertiv and Geoclima bring immense knowledge and experience to this technology partnership. The introduction of the Liebert® OFC range will provide our Data Centre customers with the complete array of chiller offerings: scroll, fixed screw, inverter screw and turbocor, enabling them to meet their efficiency targets and stay ahead of regulations.”

Paolo Ferraris, president of Geoclima said: “I am sure that the mix of Geoclima’s innovative product range together with Vertiv’s state of the art laboratories and a deep knowledge of data centre applications make this technology partnership a sure success for both our companies”.

The comprehensive Liebert® OFC range will include water-cooled models from 300 kW to 1600 kW and air-cooled models from 300 kW to 1700 kW, which are also available with freecooling and adiabatic configurations.

Existing and new customers from all over the world can thoroughly test Vertiv’s complete portfolio of thermal management products under real field conditions at the state-of-the-art Customer Experience Centre in Tognana, Italy which boasts six laboratories, including the Chiller Test Laboratory with its 1.6 MW capacity, providing the ability to test and validate performance with varying chilled water temperatures and simulate ambient conditions ranging from -10° C to +55° C, a world class indirect evaporative cooling test chamber to ensure validation of customers specified operating condition together with multiple air conditioning unit laboratories.

As part of Vertiv’s innovation roadmap, the company recently redesigned the entire floor-mount air conditioning range, including the direct expansion Vertiv™ Liebert® PDX with variable speed compressors and the chilled water range with the newly redesigned Vertiv™ Liebert® PCW.

Vertiv’s global service capabilities provides commissioning, start-up through to fully comprehensive preventative maintenance offerings, and operational energy efficiency optimisation audits.

Vertiv will be demonstrating new technologies using an augmented reality experience at Data Center World in London, stand n. D720. For more information on Vertiv’s thermal management portfolio, visit Vertiv.com.

About Vertiv

Vertiv (NYSE: VRT) brings together hardware, software, analytics and ongoing services to ensure its customers’ vital applications run continuously, perform optimally and grow with their business needs. As Architects of Continuity™, Vertiv solves the most important challenges facing today’s data centres, communication networks and commercial and industrial facilities with a portfolio of power, cooling and IT infrastructure solutions and services that extends from the cloud to the edge of the network. Headquartered in Columbus, Ohio, USA, Vertiv employs approximately 20,000 people and does business in more than 130 countries. For more information, and for the latest news and content from Vertiv, visit Vertiv.com.

CONTACT

Katie Evans
katie.evans@madebychameleon.com

Gerelateerde artikelen

PARTNERS
Overzicht
Partner-login

Taal & locatie