Working with our Vertiv Sales team enables complex designs to be configured to your unique needs. If you are an organization seeking technical guidance on a large project, Vertiv can provide the support you require.

Learn More

Many customers work with a Vertiv reseller partner to buy Vertiv products for their IT applications. Partners have extensive training and experience, and are uniquely positioned to specify, sell and support entire IT and infrastructure solutions with Vertiv products.

Find a Reseller

Already know what you need? Want the convenience of online purchase and shipping? Certain categories of Vertiv products can be purchased through an online reseller.


Find an Online Reseller

Need help choosing a product? Speak with a highly qualified Vertiv Specialist who will help guide you to the solution that is right for you.



Contact a Vertiv Specialist

Liebert Solutions Protect University’s Unique Engineering-Focused IT Needs with Increased Cooling Efficiency

июля 11, 2018

Background

Managing a data center designed to support the needs of more than 4,500 students and staff, the IT staff at the University of Maryland’s A. James Clark School of Engineering is charged with integrating the university’s enterprise IT infrastructure with the school’s unique, engineering-focused IT needs. The data center is also used to provide redundant web service for university websites and back-up services for several departmental groups, making IT system availability critical to these applications.

Results

  • Doubled cooling capacity and physical capacity of data center.
  • Optimized server configuration and airflow for maximum efficiency and IT availability.
  • Improved Power Usage Effectiveness (PUE) by 5.5 percent.

Case Summary
Location: College Park, Maryland
Critical Need: Optimize an existing data center infrastructure for efficiency, availability and space-utilization to promote availability and accommodate future IT growth.
Vertiv Solution:
  • Comprehensive Thermal Assessment with Computational Fluid Dynamics (CFD) Modeling
  • SmartAisle™ technologies, including Liebert® CRV™ Row-Based Precision Cooling Solution with Liebert iCOM™ Controls and remote monitoring facilitated by Liebert’s Virtual Ntegrity Gateway (VNG)
Download the Case Study

Статьи на похожие темы

РЕШЕНИЯ
Общая информация
Имя для входа партнера

Язык и регион